Technical FAQs

Ask a Question

What is a MBP_MSTR error 16#300B ?

Title
MBP_MSTR error 16#300B
 
Issue
MBP_MSTR error 16#300B
 
Product Line
TSXETG100, TSXETG150
 
Environment
TSXETG100, TSXETG150
 
Cause
N/A
 
Resolution
 The MBP_MSTR error 16#300B is a exception response form the remote node that means there was No response obtained from target device.
This error is typical when sending the request to a ModbusTCP to Modbus gateway where there is no response from the serial device on the Modbus side of the TSXETG100 gateway.
Was this helpful?
What can we do to improve the information ?