Technical FAQs

Ask a Question

Is there a manual for the BMXNGD0100 module ?

Title
BMXNGD0100 module manual
 
Issue
BMXNGD0100 module manual
 
Product Line
M580
 
Environment
M580
 
Cause
N/A
 
Resolution
 There is no user manual available for the BMXNGD0100 module.
The BMXNGD0100 module is configured like the BMXNOE0100 for the Global Data service.
Customer's are to reference the section on Global data in the BMXNOE0100 manual.
 
Was this helpful?
What can we do to improve the information ?