Technical FAQs

Ask a Question

Is it possible to upgrade the firmware for the Siemens Access 9340 / 9360 meters?

Issue
A customer is wanting to know if it is possible to upgrade the firmware for the Siemens Acess 9340 / 9360 series meters.

Product Line
Siemens Access 9340 /  9360 meters

Resolution
*Warning: The firmware utilities listed here can cause permanent damage to your product if applied incorrectly. Before downloading any firmware updates, verify the firmware you are downloading is appropriate for the specific model number of your product. If you have any doubts, contact Technical Support for guidance.*

*Warning: Devices should be disconnected from all monitoring software before performing a firmware upgrade*


It is possible to upgrade the meters using the DLF-3000 utility. The firmware files are attached. The files should be downloaded in the following order: RS, DL, and OS.

For more information on how to upgrade firmware using DLF-3000 software, visit article FA237920
Was this helpful?
What can we do to improve the information ?