Technical FAQs

Ask a Question

Preventa XCS - What plastic is the XCSTE safety switch casing made of?

The XCSTE safety switch casing is made of black PA66 GF25. The head uses the same material in red colour. GF25 means 25% glass fiber reinforced. PA66 stands for Polyamide 6,6 (Trade name Nylon for example).

Was this helpful?
What can we do to improve the information ?