Technical FAQs

Ask a Question

Preventa XCS - What plastic is the XCSLE safety switch casing made of?

The XCSLE safety switch casing is made of black PA66 GF25. The head uses the same material. GF25 means 25% glass fiber reinforced. PA66 stands for Polyamide 6,6 (Trade name Nylon for example).

Was this helpful?
What can we do to improve the information ?