Technical FAQs

Ask a Question

Preventa XCS - What plastic is the XCSP switch casing made of?

The plastic casing of the red XCSP safety switch is a red Valox 553, or PBT+PC GF30. PBT stands for polybutylene terephthalate, PC for polycarbonate, GF30 means 30% glass fiber reinforced.

Was this helpful?
What can we do to improve the information ?