Technical FAQs

Ask a Question

Osisense XS - What plastic is the reference XSZE212 made of?

XSZE212 is a set of 2 plastic nuts M12 for cylindrical proximity sensors XS in dia 12mm, black colour. Material is PPS GF40. GF40 means 40% glass fiber reinforced. PPS stands for Polyphenylene Sulfide  (Thermoplastic). Examples of PPS trade name = Ryton or Tecatron.

Was this helpful?
What can we do to improve the information ?