Technical FAQs

Ask a Question

Osisense XS - What plastic is the reference XSZE218 made of?

XSZE218 is a set of 2 plastic nuts M18 for cylindrical proximity sensors XS in dia 18mm, black colour. Material is PA66 GF25. GF25 means 25% glass fibre reinforced. PA66 stands for Polyamide 6,6 (Trade name Nylon).

Was this helpful?
What can we do to improve the information ?