Technical FAQs

Ask a Question

Can the ​ 'PlantStruxure General Purpose Library for Wonderware System Platform' be modified to add your own custom symbols.

Goals and Symptoms
Can the ​ 'PlantStruxure General Purpose Library for Wonderware System Platform' be modified to add custom symbols.

Facts and Change
Unity

Causes and Fixes 
Yes, the 'PlantStruxure General Purpose Library for Wonderware System Platform' can be modified to add custom symbols.
This can be accomplished by:
  • Derive the customized template from the application template.
  • Add in the new symbols to the customized template.

Note: The user must have a good knowledge of development in Wonderware Archestra.  This procedure is not provided with the library. 
Was this helpful?
What can we do to improve the information ?