Technical FAQs

Ask a Question

Osisense XC - What is the UL94 flame classification of the XCKT plastic case?

The plastic case of the XCKT limit switch is a blue Valox 553, or PBT+PC GF30. It is flame classified UL94 V-0. Attached flammability test conditions and requirements.

Was this helpful?
What can we do to improve the information ?