Browse FAQs

Preventa XCS - XCSLE353531M3 pin-out of the M23 connector.

Published date: 10 June 2019

Find attached the wiring diagram of the XCSLE353531M3 safety switch, having 1NC + 2NO main contacts and 1NC + 2NO electromagnet contacts. It is a version with locking by electromagnet on de-energisation, with M23 19-pin connector. The electromagnet contacts are represented electromagnet not energised.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.