Digital Output Tags have Bad Quality in Scada when Using ION Protocol
Issue
A device profile is created using Profile Editor based on ION protocol, and then exported to a project in PSE. A device is added to the project based on this profile. The quality for all digital output tags are 'Bad'.
Cause
The tag addresses in PSE don't match the digital output labels in the ION device.
Resolution
Find out what the output labels are for the digital output modules and modify the tag addresses accordingly. Here is an example of where to find the label for one of the digital outputs:
Once all tag addresses are modified, PSE is able to find the digital outputs:
Note that the tag addresses can either be modified in Profile Editor or using Variable Tags in Citect Project Editor.
Sign up for all the latest solutions, offers and best practices straight to your inbox.
All done!
Thank you for subscribing to updates from Schneider Electric.
We are excited that you have joined the group. You will receive your welcome email soon describing the program and what to expect in the upcoming weeks. Enjoy!