Technical FAQs

Ask a Question

Boards Address when Adding a Device to Scada with ION Protocol

Issue
An Ethernet device is added to the project using ION protocol, however, the device does not communicate.

Product Line
PowerScada Expert 8.1 (PSE 8.1)

Environment
Citect Project Editor > Boards

Cause
The 'Address' field in the Boards form is set to 0 by default.  The address for an ION meter connected through Ethernet is 100 by default.

Resolution
In the Boards form, set the address to 100.  Pack, Compile and Run the project again.

          
 
Was this helpful?
What can we do to improve the information ?