Technical FAQs

Ask a Question

What is the part number for the Magelis Panel PC Fan Kits?

Issue:
What is the part number for the Magelis Panel PC Fan Kits?

Product Line:
HMIP

Environment:


Cause:


Resolution:
There are two part numbers for the fan kits:
HMIYPFKT01 for 15" and 19" HMIPs with no PCI/ PCI Express slots
HMIYPFKT21 for 15" and 19" HMIPs with PCI/PCI Express slots
 
Was this helpful?
What can we do to improve the information ?