Technical FAQs

Ask a Question

How to navigate to the home screen in ION7650 or ION7550 with Remote Display?

Unable to go back to the home screen from a diagnostic screen of an ION7x50 remote display.

Product Line
ION7650 & ION7550 Remote Display

The buttons on the Remote Display are not as clear of their function as the integrated display.

The half circle arrow icon pointing to the left on the remote display will escape out of any screen and will go to the home screen.
This icon does the same function as the ESC button on the ION7650/7550 integrated display.

Below is a screen shot describing the functions for all the buttons on the remote display:


For more information, the ION7650/7550 Remote display Installation and User guide is attached to this article.
Was this helpful?
What can we do to improve the information ?