Technical FAQs

Ask a Question

What is the part number for additional terminal blocks for a TM2DRA16RT?

TM2DRA16RT comes with the terminal blocks. If additional terminal blocks are needed the part number for them is:
TWDFTB2T10 (10 way connector, screw terminals, sold in lots of two, you order that part number and you get two connectors)
 
Was this helpful?
What can we do to improve the information ?