Browse FAQs

Preventa XCS - XCSLE3838312 wiring diagram.

Published date: 10 June 2019

Find attached the wiring diagram of the XCSLE3838312 safety switch, having 3 NC main contacts and 3 NC electromagnet contacts. It is a version with locking by electromagnet on de-energisation. The electromagnet contacts are represented electromagnet not energised. Such diagram is supplied inside the switch.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.