Technical FAQs

Ask a Question

Power Monitoring Expert 8.1: Flag colors for Alphanumeric Display don't show the correct colors in the Web Applications

Issue
In Vista a Numeric Object with Alphanumeric Display is setup.  When the Flags are enabled, the color in Web Applications (Diagrams) doesn't follow the color in Vista regularly.

Here is an example of the problem:

          

In the following example the color in Web Applications followed the color in Vista properly:

          


Product Line
Power Monitoring Expert 8.1

Environment
Web Applications

Cause
Flag setup for a Numeric Object in Vista.

Resolution
*Warning: Take backups of any files prior to modifying them. Ensure the backups are in a location that will not be overwritten (i.e. the Desktop).*

The attached fix corrects the problem where some of the flag color transitions in Diagrams do not work properly.  

To deploy:
  1. Rename the existing realtime.js file in ..Schneider Electric\Power Monitoring Expert\system\WebReach\Scripts
  2. Copy in the new version of realtime.js
  3. Perform an IIS reset and clear the browser cache.
Was this helpful?
What can we do to improve the information ?