Technical FAQs

Ask a Question

Osisense XC - XCKM202 limit switch cross-reference.

The XCKM202 or XCKM202H29 limit switch has been completely discontinued in july 2003 (obsolete contact version). It was in fact an XCKM102 switch with some contact state indicator; see attached picture. It used the ZCKM2 special contact body. It is replaced by the XCKM102 or XCKM102H29 since 2004, having a new contact block.

Was this helpful?
What can we do to improve the information ?