Technical FAQs

Ask a Question

Osisense XC - What is the limit switch XCKM3915?

The XCKM3915 reference is a complete limit switch supplied with the ZCKMD39 3-contact block (NC+NC+NO snap action) and the ZCKD15 head.

     
Was this helpful?
What can we do to improve the information ?