Technical FAQs

Ask a Question

Osisense XC - How to order the complete limit switch XCKM1028?

The complete limit switch XCKM1028, supplied with the XE2SP2158 with gold flashed contacts (2-pole NC+NO snap action), is not available to order under this reference in 2016. You have to order the 2 sub-assemblies : ZCKM18 2-contact body + ZCKD02 head, and assemble them to get the reference XCKM1028.

Was this helpful?
What can we do to improve the information ?