Technical FAQs

Ask a Question

Osisense XC - How is supplied the screw to fix the ZCY* lever on the ZCE01 rotary head.

1) The ZCE01 or ZCE05 rotary head is supplied without any screw in the plastic bag like shown in the attached picture.


2) The ZCY* lever is supplied with the screw to fix it on the ZCE01 or ZCE05 rotary head.

Was this helpful?
What can we do to improve the information ?