Technical FAQs

Ask a Question

Osisense XM - What is the difference between the XMLR010G0T21 and XMLR010G0T25 pressure sensors ?

XMLR010G0T21 and XMLR010G0T25 pressure sensors are the same, the alone difference is the fluid entry. The "1" at the end means fluid entry G1/4 male and the "5" means G1/4 female. Such information appears in the product data sheet.
 
Was this helpful?
What can we do to improve the information ?