Technical FAQs

Ask a Question

What size fuse do I use for the BMXCPS2000 @ 115VAC?

We reccommend three times the CPS I2T rating. The I2T rating for 120VAC is .5A (read as point 5). 
So that suggests a fuse rating of 1.5 Amp. (normal blo)




R-71317
Was this helpful?
What can we do to improve the information ?