Technical FAQs

Ask a Question

SPM/PME: Server Error in '/Web' Application - Could not load type 'System.ServiceModel.Activation.HttpModule

Issue
An attempt to login to the Web Application prompts with the following error:

Server Error in '/Web' Application.
--------------------------------------------------------------------------------

Could not load type 'System.ServiceModel.Activation.HttpModule' from assembly 'System.ServiceModel, Version=3.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089'. 
Description: An unhandled exception occurs during the execution of the current web request. Please review the stack trace for more information about the error and where it originated in the code. 

Exception Details: System.TypeLoadException: Could not load type 'System.ServiceModel.Activation.HttpModule' from assembly 'System.ServiceModel, Version=3.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089'.

Source Error: 

An unhandled exception is generated during the execution of the current web request. Information regarding the origin and location of the exception can be identified using the exception stack trace below.  

Stack Trace: 

[TypeLoadException: Could not load type 'System.ServiceModel.Activation.HttpModule' from assembly 'System.ServiceModel, Version=3.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089'.]
   System.RuntimeTypeHandle.GetTypeByName(String name, Boolean throwOnError, Boolean ignoreCase, Boolean reflectionOnly, StackCrawlMarkHandle stackMark, IntPtr pPrivHostBinder, Boolean loadTypeFromPartialName, ObjectHandleOnStack type) +0
   System.RuntimeTypeHandle.GetTypeByName(String name, Boolean throwOnError, Boolean ignoreCase, Boolean reflectionOnly, StackCrawlMark& stackMark, IntPtr pPrivHostBinder, Boolean loadTypeFromPartialName) +153
   System.Type.GetType(String typeName, Boolean throwOnError, Boolean ignoreCase) +63
   System.Web.Compilation.BuildManager.GetType(String typeName, Boolean throwOnError, Boolean ignoreCase) +124
   System.Web.Configuration.ConfigUtil.GetType(String typeName, String propertyName, ConfigurationElement configElement, XmlNode node, Boolean checkAptcaBit, Boolean ignoreCase) +76

[ConfigurationErrorsException: Could not load type 'System.ServiceModel.Activation.HttpModule' from assembly 'System.ServiceModel, Version=3.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089'.]
   System.Web.Configuration.ConfigUtil.GetType(String typeName, String propertyName, ConfigurationElement configElement, XmlNode node, Boolean checkAptcaBit, Boolean ignoreCase) +12425644
   System.Web.Configuration.Common.ModulesEntry.SecureGetType(String typeName, String propertyName, ConfigurationElement configElement) +69
   System.Web.Configuration.Common.ModulesEntry..ctor(String name, String typeName, String propertyName, ConfigurationElement configElement) +62
   System.Web.HttpApplication.BuildIntegratedModuleCollection(List`1 moduleList) +299
   System.Web.HttpApplication.GetModuleCollection(IntPtr appContext) +1262
   System.Web.HttpApplication.RegisterEventSubscriptionsWithIIS(IntPtr appContext, HttpContext context, MethodInfo[] handlers) +133
   System.Web.HttpApplication.InitSpecial(HttpApplicationState state, MethodInfo[] handlers, IntPtr appContext, HttpContext context) +304
   System.Web.HttpApplicationFactory.GetSpecialApplicationInstance(IntPtr appContext, HttpContext context) +404
   System.Web.Hosting.PipelineRuntime.InitializeApplication(IntPtr appContext) +475

[HttpException (0x80004005): Could not load type 'System.ServiceModel.Activation.HttpModule' from assembly 'System.ServiceModel, Version=3.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089'.]
   System.Web.HttpRuntime.FirstRequestInit(HttpContext context) +12618980
   System.Web.HttpRuntime.EnsureFirstRequestInit(HttpContext context) +159
   System.Web.HttpRuntime.ProcessRequestNotificationPrivate(IIS7WorkerRequest wr, HttpContext context) +12458597

Product Line
StruxureWare Power Monitoring 7.0.x
Power Monitoring Expert 7.2.x
Power Monitoring Expert 8.x
Internet Explorer 10, 11

Environment
Power Monitoring Expert Web Applications

Cause

This issue occurs because the Applicationhost.config file for Windows Process Activation Service (WAS) has the following section defined, which is incompatible with the .NET Framework 4.0:

<add name="ServiceModel" type="System.ServiceModel.Activation.HttpModule, System.ServiceModel, Version=3.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089" preCondition="managedHandler" />

This section should be defined as follow:

<add name="ServiceModel" type="System.ServiceModel.Activation.HttpModule, System.ServiceModel, Version=3.0.0.0, Culture=neutral, PublicKeyToken=b77a5c561934e089" preCondition="managedHandler,runtimeVersionv2.0" />

Note: You can find the Applicationhost.config file in the following location: %windir%\system32\inetsrv\config

which may be caused by recent installation and/or modification of HTTP Activation role within .NET Framework.

Resolution
*Warning: Synchronizing ASP.NET with Struxureware Power Monitoring/Power Monitoring Expert software may interfere with other software utilizing ASP.NET on the same machine.

1. Open the command prompt via the Windows start menu.

2. Navigate to one of the following directories based on the type server.

%windir%\Microsoft.NET\Framework\v4.0.30319

%windir%\Microsoft.NET\Framework64\v4.0.30319 (on a 64-bit computer)

E.g. command line: 'cd %windir%\Microsoft.NET\Framework64\v4.0.30319'

3. Run the following command line: 
'aspnet_regiis.exe /iru'

This command re-installs ASP.NET.


 

Was this helpful?
What can we do to improve the information ?