Browse FAQs

Does Schneider Electric offer motor model BRX184 ?

Published date: 03 October 2018

The motor type BRX184 and all variations of this type are specialized products for our European customer W&H (Windmoeller & Hoelscher) , an OEM machine builder of printing machines. 

This motor is not available directly from Schneider Electric. 
W&H has a contract with our factory which states that this motor type is proprietary to W&H and the contract restricts the sale of this product to anyone other than W&H. 

Customers must contact W&H (Windmoeller & Hoelscher), the original machine builder, to order spare BRX184 motors

Rev 10-3-18

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.