Technical FAQs

Ask a Question

Starline M40 Specification and Modbus Registers

Issue
Electrical specification and Modbus registers

Product Line
Starline M40

Environment
User Manual

Cause
Finding information about Starline M40 power monitor widely used in Data Centers

Resolution
The attached document has information on:

- electrical parameters
- input ratings
- connector pinout
- accuracy
- operating conditions
- meter certification
- modbus registers

 
Was this helpful?
What can we do to improve the information ?