How to use Read_Var block with BMXNOC0401 communication module?
See below example of Read_Var block for reading modbus slave data through ETG100.
In ADDM block
3 is the slot adress of NOC module in the rack
192.168.0.20 is the IP address of TSXETG100 gateway.
1 is the modbus slave id
TCP.MBS for addressing a TCP Modbus server
In Read_Var block
’%MW’: for reading holding registers
Num: Index of the first object to read
NB: Number of objects to read
For more details check attached unity help documents.
Sign up for all the latest solutions, offers and best practices straight to your inbox.
All done!
Thank you for subscribing to updates from Schneider Electric.
We are excited that you have joined the group. You will receive your welcome email soon describing the program and what to expect in the upcoming weeks. Enjoy!