Technical FAQs

Ask a Question

Osisense XC - What is the material of the spring rod with thermoplastic end head ZCE07 or ZCEA7?

The spring rod with thermoplastic end head ZCE07 or ZCEA7, uses a spring made of stainless steel SUS 304 or AISI 304, without any surface threatment. The thermoplastic end is in polyamide PA6. The ZCE07 or ZCEA7 head can be associated to the following XC limit switches XCKD, XCKP, XCKT & XCMD.

Was this helpful?
What can we do to improve the information ?