Technical FAQs

Ask a Question

Osisense XC - What is the material of the "cat's whisker" head ZCE06 or ZCEA6?

The "cat's whisker" head ZCE06 or ZCEA6 uses a spring made of stainless steel SUS 304 or AISI 304, without any surface threatment. The ZCE06 or ZCEA6 head can be associated to the following XC limit switches XCKD, XCKP, XCKT & XCMD.

Was this helpful?
What can we do to improve the information ?