Technical FAQs

Ask a Question

Osisense XC - What is the material of the spring rod head ZCE08 or ZCEA8?

The spring rod head ZCE08 or ZCEA8 uses a spring made of stainless steel closed to the SUS 302 or AISI 302, without any surface threatment. The ZCE08 or ZCEA8 head can be associated to the following XC limit switches XCKD, XCKP, XCKT & XCMD.

Was this helpful?
What can we do to improve the information ?