Browse FAQs

What is the difference between the B875-001 and B875-002 modules?

Published date: 27 September 2018

The B875-002 module has either 4 or 8 individually isolated analog input channels. It has dip switches that allows you the option to setup for either 4-channel or 8-channel mode. The older B875-001 module was strictly an 8 channel analog input module. If you wanted 4-channels, you would use the B873-001 module.

Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.