Technical FAQs

Ask a Question

Preventa XU - What is the XUSLZ450 reference? Cross-reference in 2016?

The XUSLZ450 reference was the CD-ROM supplied with the obsolete XUSLT, XUSLM, XUSLP, XUSLN, XUSLB, XUSLD safety light curtains, providing the user manuals. Different versions existed. In 2015, it is no more available to order because of the concerned light curtains obsolescence. How to replace in the XUSL4E & XUSL2E light curtain offer : use the "" site to download the corresponding alone user manual at following @

Was this helpful?
What can we do to improve the information ?