Technical FAQs

Ask a Question

Osisense XS_XS7C4A1DPG13TF data sheet.

Find attached the datasheet of the XS7C4A1DPG13TF adapted sensor, not shown in the Osisense XS catalogue. The TF suffix meaning is extended low temperature range to -40°C in operation. The sales of such product are open for all customers in 2016. It is not in stock (produced at order reception).
Was this helpful?
What can we do to improve the information ?