Technical FAQs

Ask a Question

Can I purchase the display or Control unit of a HMISTU655 or HMISTU855 separately?

You can purchase the HMISTU655 or HMISTU855 as a complete unit or the rear module and screen separately.

HMISTU655 Complete unit 3.5"
HMISTU855 Complete unit 5.7"

HMIS5T Rear module only

HMIS65 3.5" Front display only
HMIS85 5.7" Front display only


 
Was this helpful?
What can we do to improve the information ?