Technical FAQs

Ask a Question

How to allow the tranfer of a Web Designer project on a BMENOC0311 module?

Title
Web Designer project transfer to a BMENOC0311 module
 
Issue
Web Designer project transfer to a BMENOC0311 module
 
Product Line
BMENOC0311
 
Environment
Web Designer
 
Cause
N/A
 
Resolution
To transfer a Web Designer project to the BMENOC0311 module. using latest firmware and Web Designer version requires that the Access Management Security be turned Off.
Use the following steps to resolve the issue:
-Open the Setup web page on the BMENOC0311
-Click on Access Management
-Click on the ‘Off’ button to disable Access Management.

After transfer of the Web Designer project, the user should enable the Access Management Security by setting it back to ON.
Was this helpful?
What can we do to improve the information ?