Browse FAQs

Does Schneider Electric offer a suitable replacement for Twinline stepping motor power cable type TLACPVAA0051 ?

Published date: 16 September 2019

Yes, the Twinline power cable type TLACPVAA0051 is available using a new part number.

The stepping motor power cables for the Schneider Electric SD3 product line are the same cables as those which were previously included in the Twinline accessory product line, only now the part numbers have been changed

To replace TLACPVAA0051 use the new reference number of VW3S5101R50.  
This will be a 5 meter long 3 phase stepping motor power cable


Other lengths are available, if needed, as seen in the attached list of stepping motor power cables. 


Rev 9-14-17

Was this helpful?

What can we do to improve the information ?