Technical FAQs

Ask a Question

Does Schneider Electric offer a suitable replacement for Lexium Integrated drive type ILS1F852S1449 ?

No, the Lexium Integrated drive with type code ILS1F852S1449 is an OEM specific model which must be ordered from the OEM machine builde.
This model has design features unique to the OEM machine builder and because of this is considered a proprietary model which is only sold to the OEM.
Therefore, cuttomers looking to replace this model must contact the OEM machine builder for spares.

rev 9-14-17
Was this helpful?
What can we do to improve the information ?