Technical FAQs

Ask a Question

Certification according to North American Standards (UL, CSA…)

Certification according to North American Standards (UL, CSA…)
 
 
The FAQ takes, as an example, the case of a Certification against the UL standard. Could be CSA or other.
 
When a certification according to an UL standard is requested by the clients, it is often that the clients expect to receive a Certificate published by the UL and to see the UL marking on the label of the product.
 
For some products, Schneider Electric has asked the UL to test our products for UL certification : in this case, the certificate will effectively be published by the UL and we will put the UL marking on the products.
However, this is absolutely not mandatory and it is normal that Schneider Electric also asks any other officially recognized Laboratory to test our products against an UL standard..
Below attached in PDF is a brief explanation about this topic.
 
Was this helpful?
What can we do to improve the information ?