Technical FAQs

Ask a Question

What is the difference between Modbus+ driver Suite V8.1 and V8.0

The only difference between Modbus+ driver Suite V8.1 and V8.0 is that V8.1 supports the new hardware Modbus+ PCI Express (or PCIe) 416NHM30042A for PC's.
 
Was this helpful?
What can we do to improve the information ?