Technical FAQs

Ask a Question

PME 8.1 Data Center Edition Vista Fails to Load User Diagrams

Issue
When clicking open an existing user diagram in Vista, in the status bar it says: "Loading aborted".

Product Line
Power Monitoring Expert 8.1 DC 

Environment
Vista

Cause
This occurs when PME8.1 DC is installed on Windows Server 2008 R2 without the Windows Service Packs applied.

Resolution
Install Service Pack 1 for Windows Server 2008 R2 and restart the server. 

For more information on installing Service Pack 1 for Windows Server 2008 R2 see the following link:
https://technet.microsoft.com/en-ca/windows/gg635126.aspx
 
Was this helpful?
What can we do to improve the information ?