Technical FAQs

Ask a Question

Does the Quantum product Ethernet ports have the bility to ping a remote device connected PLC via ethernet?

Title
Quantum Ethernet port ping capability
 
Issue
Quantum Ethernet port ping capability
 
Product Line
Quantum
 
Environment
Unity
 
Cause
N/A
 
Resolution
The Quantum CPU Ethernet port nor the 140NOE771x1 module have the ability to ping remote nodes from within the Unity software or from their webpages.
Was this helpful?
What can we do to improve the information ?