Technical FAQs

Ask a Question

What is the Connexium Network Manager software?

Title
Connexium Network Manager
 
Issue
Connexium Network Manager
 
Product Line
Connexium Network Manager
 
Environment
N/A
 
Cause
N/A
 
Resolution
 The ConneXium Network Manager (CNM) provides a solution for configuring and monitoring the administrative Schneider Electric devices, including switches, firewalls, ConneXium Wifi devices and products from various manufacturers.
The standardized LLDP protocol is used to scan network infrastructure components and the received information allows CNM to build a representation of the network connectivity. End devices such as PLCs, I/O, and HMIs are also detected and their location is accurately depicted on the graphical topology map. CNM software enables you to detect unmanaged switches and hubs and display their position within your network diagram. The software is also able to determine the network topology of devices which are located behind a router. This results in an increased level of topology detail.
 
Was this helpful?
What can we do to improve the information ?