Technical FAQs

Ask a Question

Can the HMISCU temperature inputs be wired for standard 4-20mA analog input?

 Issue:
Can the HMISCU temperature inputs be wired for standard 4-20mA input?

Product Line:
HMISCU8B5, HMISCU6B5, HMISCU8A5, HMISCU6A5

Environment:


Cause:


Resolution:
That is not possible, the temperature inputs can not be used as standard analog inputs.  The recommendation would be to use Advantys OTB island with an analog input module (TM2AMI2HT or TM2AMI8HT).

 
Was this helpful?
What can we do to improve the information ?