Browse FAQs

What is the replacement of the Magelis XBTG5230?

Published date: 22 October 2018

XBTG5230 has been replaced with the HMIGTO6310

    • Vijeo Designer applications are 100 % compatible with automatic screens resizing.
      The cut-out is identical.
      The communication ports are identical except on COM1 , no RS422 signal only RS232C
      Same certifications.
      Only one USB port Host type A
      No auxiliary interface for speaker or alarm output
      Better Screen color TFT 65K and bigger Screen Size 12.1-inch , More Flash Memory , addition mini-USB Device port and use of SD card slot.


Was this helpful?

What can we do to improve the information ?

Can't find what you are looking for?

Reach out to our customer care team to receive information on technical support, assistance for complaints and more.