Technical FAQs

Ask a Question

Magelis HMIG3U locking up when running Vijeo Designer v6.2 runtime. How to resolve the issue?

Issue:
Magelis HMIG3U locking up when running Vijeo Designer v6.2 runtime. How to resolve the issue?

Product Line:
HMIGTU, freeze, lock

Environment:


Cause:


Resolution:
There were some performance issues with the Mageis HMIG3U targets causing it to lock up or freeze.  But the issue was resolved in SP4.1 for Vijeo Designer v6.2.  Please contact Schneider Electric for the link to Vijeo Designer service packs.  Even though SP4.1 fixes that issue but it is recommended that you upgrade to the latest service pack.
 
Was this helpful?
What can we do to improve the information ?