Technical FAQs

Ask a Question

What revision of Quantum product firmware corrects CERT alerts?

Schneider Electric takes security very seriously and responds to threats as soon as possible. Security alerts are issued by the CERT Division of the Software Engineering Institute (SEI). These are usually addressed by firmware changes to our product. The attached chart indicated the number of the CERT Alert and the revision of the firmware that deals with it for Quantum communication products. The information is valid as of Aug 29, 2016.
Was this helpful?
What can we do to improve the information ?