Technical FAQs

Ask a Question

What is the part number of the Quantum Unity Double Wide Modbus programming cable?

The part number of the Quantum Unity Double Wide Modbus programming cable is a 110XCA20300 (DB9 - RJ45 Adapter) and one of the below 110XCA2820X  communication cable depending of length needed:

110XCA28201 RS232 Communication Cable—3ft, RJ45–RJ45.
110XCA28202 RS232 Communication Cable—10ft, RJ45–RJ45.
110XCA28203 RS232 Communication Cable—20ft, RJ45–RJ45.
Was this helpful?
What can we do to improve the information ?