Technical FAQs

Ask a Question

Unity Pro 11 and lower, error message on Upload or import {{ 0.0 - BME P58 xxxx } The selected processor doesn't support such a number of %Mi

The maximum number of %M is limited to 32634 on M580 CPU 5810xx, 5820xx, 5830xx, but it is limited to 32624 on M580 CPU 5840xx , 5850xx, 5860xx
Although it seems possible to configure up to 32634 %M on M580 CPU 5840xx , 5850xx, 5860xx, the import or upload of such application will fail.

On Unity Pro V11.1 such application could not be built. the right size will have to be put.

Was this helpful?
What can we do to improve the information ?