Technical FAQs

Ask a Question

Is it possible to configure M580 redundant CPU and BMENOC03x1 both as FDR server in M580 HSBY

In an M580 Hot Standby system, either the BMEH58•040 CPU or a BMENOC03•1 Ethernet communication module can perform the role of an FDR server.
To do so enable the TFTP service in the CPU.

Was this helpful?
What can we do to improve the information ?